Protection circuit between VSNVS and VDD_SNVS_IN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Protection circuit between VSNVS and VDD_SNVS_IN

ソリューションへジャンプ
1,832件の閲覧回数
ko-hey
Senior Contributor II

Hi all

I plan to use i.MX6ULL and PF3000 and want to confirm that I need to add a protection circuit between VSNVS and VDD_SNVS_IN.

We connects to VSNVS and VDD_SNVS_IN.

Furthermore, coin batteries may not be installed in some cases, and the VIN power to be supplied to the PF3000 is not a battery but an AC adapter, so there are situations where the power supply at the base can be suddenly cut off.

Here is the description in the Hardware Development Guide.

When VDD_HIGH_IN > VDD_SNVS_IN

VDD_HIGH_IN supplies all SNVS domain current and current flows into VDD_SNVS_IN to charge a coin cell battery.

From the above description, I think that user need to have a protection circuit for backflow prevention.

Am I correct ?

Ko-hey

ラベル(3)
0 件の賞賛
返信
1 解決策
1,569件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  generally You are right; note it is enough to use a diode to prevent current flow

(if present) from VDD_HIGH_IN via  VDD_SNVS_IN to charge a coin cell battery.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,570件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  generally You are right; note it is enough to use a diode to prevent current flow

(if present) from VDD_HIGH_IN via  VDD_SNVS_IN to charge a coin cell battery.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信