Programming SJC_DISABLE, JTAG_SMODE and JTAG_HEO fuses on iMX8MM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programming SJC_DISABLE, JTAG_SMODE and JTAG_HEO fuses on iMX8MM

ソリューションへジャンプ
4,662件の閲覧回数
rodrigo_travess
Contributor I

Hello,

At the AN4581 Application Note section 5.7 it is recommended to program the SJC_DISABLE, JTAG_SMODE and JTAG_HEO fuses to completely secure the device, but looking at both the IMX8MMRM and IMX8MMSRM, I wasn't able to find the exact location of those fuses (bank, word, bit). Where can I find this information?

Thank you!

0 件の賞賛
返信
1 解決策
4,645件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi rodrigo_travess

 

additional info were sent via mail.

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
9 返答(返信)
1,257件の閲覧回数
tsmt
Contributor II

We also would like to have this information.

0 件の賞賛
返信
4,026件の閲覧回数
jxb4256
Contributor II

Can you also share this with me, please? Why isn't this just posted in a public app note, or the reference manual or security reference manual? Security through obscurity is not security.

4,521件の閲覧回数
stephanwächter
Contributor I

We also want to disable JTAG on the imx8m-mini and I couldn't find any info of about it in Reference Manual, Rev. 2, 08/2019 Chapter 6.2 Fusemap. Could you also point me into the right direction.

Thank you!

0 件の賞賛
返信
4,646件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi rodrigo_travess

 

additional info were sent via mail.

 

Best regards
igor

0 件の賞賛
返信
394件の閲覧回数
dj_RS
Contributor I

Hi @igorpadykov ,

I would appreciate if you could send me this information as well.

Thanks in advance

Dj

0 件の賞賛
返信
1,149件の閲覧回数
emmanuel_madrigal
Contributor I

Hi,

 

Would it be possible for you to send me this information as well?

 

Also is this diifferent between an imx8m nano  and a mini?

0 件の賞賛
返信
2,618件の閲覧回数
jbruno79
Contributor I

hi @igorpadykov,

I need information about the fuses for the imx8m mini. Could you be so kind to provide it to me? I need to disable the JTAG for security reasons.

Best regrads,

Julián

0 件の賞賛
返信
3,115件の閲覧回数
johneubanks
Contributor I

@igorpadykov could you also send me the info for the JTAG_HEO fuse?
Thanks!

0 件の賞賛
返信
4,360件の閲覧回数
paul_geurts
Contributor III

Could you make this email public information? Why is this information not listed in the security reference manual? For the i.MX8M Nano this is listed in the security reference manual. But I cannot know whether the Mini uses the same fuses.

Also, AN4581 also lists fuse DIR_BT_DIS to be of interest. But I cannot find any reference of it.

0 件の賞賛
返信