Hi,
I am using Linux 2.6.35.03 kernel. I am working on FlexCAN. I had installed "canutils" and "libsocket". But i am not able to set the bitrate with following command
ip link set can0 type can bitrate 125000
it was showing following error
RTNETLINK answers: operation not supported
I posted the query and I got patch from the Community. Could you please tell me the procedure to apply patch for kernel
I have attached the patch
Original Attachment has been moved to: linux-2.6.35_mainline_flexcan.patch.zip
Hi Karthikeyan
https://community.nxp.com/thread/299202
also for general procedure applying patches please refer to attached document
p.3 from L2.6.35_11.09 documentation.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------