According to the NXP information: (UM11583) Getting Started with the 88Q9098/88W9098 Evaluation Board.
I have tried to test the Wi-Fi /BT module 88Q9098 in IMX6Q-SDB.
The kernel version is L5.10.72_2.2.0.
I have some questions:
(1) I use iperf3 to test Wi-Fi transmission from the EVK board to PC or smartphone (Android).
If the EVK board is the client to transmit packets, the transmission rate may drop from time to time whether is related to imx6 and 9098?
(2) I tried adding "main.conf" in "/etc/bluetooth/" and modifying the class and name, but it didn't work. Besides, I used to try using A2DP, and it also didn't work.
Do you have any way for me to be sure to receive or transmit data to a smartphone or PC via Bluetooth? (e.g. txt, jpeg)