Problems with programming nk.nb0 with ATK Toolkit and i.MX35

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems with programming nk.nb0 with ATK Toolkit and i.MX35

2,899 Views
fossi15
Contributor I

Hello,

at this moment, i use the ATK Toolkit 1.71 to program the XLDR.nb0 and the Eboot.nb0 to the i.MX. The Kernel, i am programing with Platform builder to the i.MX. This is working fine.

But in future, the programming of our board will do some guys in production department. Because these guys did not have Platform Builder, they have to use the ATK to program the nk.nb0 to i.MX.

I tested now the programming of the Kernel with ATK and have now the problem, that the Kernel will not load from NAND-Flash to RAM and so, the Kernel will not start. What could be my fault of thinking?

For some helpfull answers i will much obliged!

Greetings,

Norbert

Labels (3)
0 Kudos
Reply
3 Replies

2,098 Views
KeshavaGN
Contributor V

Hi all,

You can download CeLoader.exe from this link: Simple TFTP loader for Windows Embedded Compact EBOOT - Download Release File

With regards,

Keshava G N

0 Kudos
Reply

2,098 Views
Yuri
NXP Employee
NXP Employee

The NK file cannot be downloaded with ATK tool.

To deploy images You may try ideas, suggested in the topic, linked below.

("Flashing a Windows CE 5.0 Device Without Using Platform Builder")

http://msdn2.microsoft.com/en-us/library/aa446908.aspx

The following should be done for it:


1.

We should apply TFTP client program, that may be configured for different ports

(standard TFTP port is 69). As was mentioned in the topic, the TFTP server in

the EBOOT boot loader uses non-standard TFTP port 980.

For example, WinAgents TFTP Client program may be used.

http://www.winagents.com/en/products/tftp-client/index.php 


2.

EBOOT bootloader file ("Eboot.nb0") may be loaded and run on the board, using

external JTAG debugger or ATK toolkit


3.

Configure  EBOOT to use static (non-DHCP) IP address, say, 192.168.2.75. 


4.

Select EBOOT option "D) Download image now".


5.

Run tftp.exe to send the CE image (NK.BIN) to the board's IP address as follows:

"TFTP1 -i -p980 192.168.2.75 PUT BOOT.BIN".

Any file (in WinCE .bin format) to be loaded via EBOOT should be renamed as

"BOOT.BIN". 

2,098 Views
norbertpeter
Contributor I

Hello Mr. Muhin,

thank you for your answer! Yesterday, I found in the Web a program CeLoader.exe, which is solving my problem!

Bye and with best regards,

Norbert Peter

0 Kudos
Reply