Hi, help me!
I have some problems building the system 4.19.35 for imx6ull when I using the instructions i.MX_Yocto_Project_User's_Guide.
I'm using ubuntu 18.04.
I follow these steps:
1. Installed packages:
sudo apt-get install gawk wget git-core diffstat unzip texinfo gcc-multilib build-essential chrpath socat cpio python python3 python3-pip python3-pexpect xz-utils debianutils iputils-ping python3-git python3-jinja2 libegl1-mesa libsdl1.2-dev pylint3 xterm
2. I'm setting up a repo package:
mkdir ~/bin
curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo
chmod a+x ~/bin/repo
sudo apt-get install repo
3. I'm setting up a Yocto project
git config --global user.name "Your Name"
git config --global user.email "Your Email"
git config –list
mkdir imx-yocto-bsp
cd imx-yocto-bsp
repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-warrior -m imx-4.19.35-1.1.0.xml
repo sync
4.After that, I set up a build configuration
MACHINE=imx6ull14x14evk DISTRO=fsl-imx-fb source fsl-setup-release.sh -b build_ull
5. Started build
bitbake imx-image-multimedia
Thus, I got a tree of devices and a system image that are in the folder tmp/deploy/images/imx6ull14x14evk
6. After which I change the device tree, for the test I changed lsd in the file:
tmp/work-shared/imx6ull14x14evk/kernel-source/arch/arm/boot/dts/imx6ull-14x14-evk.dts
tmp/work/cortexa7t2hf-neon-poky-linux-gnueabi/linux-libc-headers/4.19-r0/linux-4.19/arch/arm/boot/dts/imx6ull-14x14-evk.dts
/home/sasha/imx-yocto-bsp/build_ull/tmp/work/imx6ull14x14evk-poky-linux-gnueabi/linux-imx/4.19.35-r0/git/arch/arm/boot/dts/imx6ull-14x14-evk.dts
7. I start build again
bitbake imx-image-multimedia
8. Checking files in
tmp/deploy/images/imx6ull14x14evk
but they have not changed and in the terminal I see the following:
NOTE: Tasks Summary: Attempted 5720 tasks of which 5720 didn't need to be rerun and all succeeded.
What am I doing wrong?
I also tried using commands:
bitbake imx-image-multimedia -с fetch
bitbake imx-image-multimedia -с deploy
bitbake imx-image-multimedia -c compile -f
but it did not bring the desired result.
Regards,
Aleksandr
已解决! 转到解答。
After you change the device tree or just the kernel code, you need not compile the full image.
Try below command and check the dtb and zImage:
$ bitbake -c compile -f linux-imx
$ bitbake linux-imx
Regards,
Karan Gajjar
Hello Aleksandr,
Karan Gajjar’s suggestion is a good one. However, there is also the fact that Yocto is designed around distribution and not development. This means that Yocto does not keep track of changed source files and that sometimes the recipe will re-fecth the original configuration, erasing your changes.
It is suggested that you work on the changed you require by cross compiling outside of Yocto and that you incorporate the changes trough new recipes or appends to the current recipes. You can find more information on the Yocto Project documentation.
Regards,
After you change the device tree or just the kernel code, you need not compile the full image.
Try below command and check the dtb and zImage:
$ bitbake -c compile -f linux-imx
$ bitbake linux-imx
Regards,
Karan Gajjar