Dear community,
We occured the following problems during testing on the reference SABRESD board(MCIMX6Q-SDB).
Problems with CS1 control fail when using EIM interface in u-boot
** Questions **
- Is the below setting correct?
- In kernel, success to write data to EIM CS0 / CS1 using ioremap function.
In uboot environment, how to write data to an address without ioremap function?
The environment and settings are shown below.
1. uboot version : v2013.10-r0
2. Kernel version : L3.0.35-r37.14
3. modify u-boot source code
- file : board/freescale/mx6sabresd
- function : board_late_init()
- PAD Setting
iomux_v3_cfg_t weim_pads[] = {
MX6_PAD_EIM_OE__WEIM_WEIM_OE | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_RW__WEIM_WEIM_RW | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_CS0__WEIM_WEIM_CS_0 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_CS1__WEIM_WEIM_CS_1 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_LBA__WEIM_WEIM_LBA | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_BCLK__WEIM_WEIM_BCLK | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_EB1__WEIM_WEIM_EB_1 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_DA15__WEIM_WEIM_DA_A_15 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_DA14__WEIM_WEIM_DA_A_14 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_DA13__WEIM_WEIM_DA_A_13 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_DA12__WEIM_WEIM_DA_A_12 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_DA11__WEIM_WEIM_DA_A_11 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_DA10__WEIM_WEIM_DA_A_10 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_DA9__WEIM_WEIM_DA_A_9 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_DA8__WEIM_WEIM_DA_A_8 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_DA7__WEIM_WEIM_DA_A_7 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_DA6__WEIM_WEIM_DA_A_6 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_DA5__WEIM_WEIM_DA_A_5 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_DA4__WEIM_WEIM_DA_A_4 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_DA3__WEIM_WEIM_DA_A_3 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_DA2__WEIM_WEIM_DA_A_2 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_DA1__WEIM_WEIM_DA_A_1 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_DA0__WEIM_WEIM_DA_A_0 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_CSI0_DAT12__WEIM_WEIM_D_8 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_CSI0_DAT13__WEIM_WEIM_D_9 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_CSI0_DAT14__WEIM_WEIM_D_10 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_CSI0_DAT15__WEIM_WEIM_D_11 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_CSI0_DAT16__WEIM_WEIM_D_12 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_CSI0_DAT17__WEIM_WEIM_D_13 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_CSI0_DAT18__WEIM_WEIM_D_14 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_CSI0_DAT19__WEIM_WEIM_D_15 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_A16__WEIM_WEIM_A_16 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_A17__WEIM_WEIM_A_17 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_A18__WEIM_WEIM_A_18 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_A19__WEIM_WEIM_A_19 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_A20__WEIM_WEIM_A_20 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_A21__WEIM_WEIM_A_21 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_A22__WEIM_WEIM_A_22 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_A23__WEIM_WEIM_A_23 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_A24__WEIM_WEIM_A_24 | MUX_PAD_CTRL(EIM_PAD_CTRL),
MX6_PAD_EIM_A25__WEIM_WEIM_A_25 | MUX_PAD_CTRL(EIM_PAD_CTRL)
};
imx_iomux_v3_setup_multiple_pads(weim_pads,ARRAY_SIZE(weim_pads));
- IOMUXC_GPR1 / CS1GCR1 / CS1GCR2 / CS1RCR1 / CS1RCR2 / CS1WCR1 / CS1WCR2 / CS1WCR Setting
void __iomem *eim_reg = MX6_IO_ADDRESS(WEIM_BASE_ADDR +0x18);
//GPR1 register/////////////////////////////////////////////////////////////////////
reg = readl(IOMUXC_BASE_ADDR + 0x4); // GPR1 register CS0/CS1 enable
reg &= ~0x07ffffff;
reg |= 0x1b;
writel(reg, IOMUXC_BASE_ADDR + 0x4);
//CS1GCR1///////////////////////////////////////////////////////////////////////////
writel(0x00051081,eim_reg); //CS1GC[18:16](DSZ -> 101 : 8bit port resides on DATA[15:8]
//CS1GCR2///////////////////////////////////////////////////////////////////////////
writel(0x00000000,(eim_reg+ 0x4)); //CS1GCR2
//CS1RCR1///////////////////////////////////////////////////////////////////////////
writel(0x16000202,(eim_reg+ 0x8)); //CS1RCR1
//CS1RCR2///////////////////////////////////////////////////////////////////////////
writel(0x00000002,(eim_reg+ 0xC)); //CS1RCR2
//CS1WCR1///////////////////////////////////////////////////////////////////////////
writel(0x16002082,(eim_reg+ 0x10)); //CS1WCR1
//CS1WCR2///////////////////////////////////////////////////////////////////////////
writel(0x00000000,(eim_reg+ 0x14)); //CS1WCR2
//CS1WCR////////////////////////////////////////////////////////////////////////////
writel(0x00000000,(eim_reg+ 0x90)); //CS1WCR
- Data Write
*(unsigned char *)(0x8400000) = 0x0A; // CS0
*(unsigned char *)(0xC400000) = 0x0A; // CS1
4. How to check the operation
- Check EIM CS1(R627) operation using oscilloscope
5. Test result
- EIM CS1 pin does not move
- When writing data (*(unsigned char *)(0x8400000) = 0x0A;) ,
uboot init no longer proceeds and kernel is not loaded.
Dear igor,
Thank you for quickly response.
In the kernel, both CS0 and CS1 are successfully written.
So in uboot, We set the same value as in Kernel for the following registers.
IOMUXC_GPR1 / CS1GCR1 / CS1GCR2 / CS1RCR1 / CS1RCR2 / CS1WCR1 / CS1WCR2 / CS1WCR
We want to access EIM CS1 using the ioremap function as in the kernel.
We understand that to use the ioremap function, we must enable the MMU.Is right?
Please let us know, How can We enable the MMU in uboot?
Dear Igor,
Thank you for your answer.
We have worked again with the eim paralle nor example in mx6qsabreauto.c file.
We use CS0 (64MB), CS1 (64MB) and write data to CS0 and CS1 respectively as shown below.
CS0 write succeeds, but a fault occurs when writing to CS1.
* (unsigned char *) (0x8400000) = 0x0A; // CS0 Write -> Success
udelay (100);
* (unsigned char *) (0xC400000) = 0x0A; // CS1 Write -> Fail
In Kernel, write is successful in both CS0 and CS1 using ioremap function.
Is there anything else I need to do to write using CS1 in uboot?
If enable MMU in uboot, can ioremap be used?
if so, Is there a way to enable the MMU in uboot?
Thank you for your help.
Hi HAE
parallel nor is used with eim on sabre ai board and one can look at its uboot:
uboot/board/freescale/mx6qsabreauto/mx6qsabreauto.c
uboot-imx.git - Freescale i.MX u-boot Tree
In particular one can check if eim clock is enabled in CCM_CCGR6
As SABRESD board (MCIMX6Q-SDB) uses EIM signals for other
purposes, one needs to check uboot code and remove EIM signals from
usage by other modules.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------