Problems encountered using UUU to burn i. MX8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems encountered using UUU to burn i. MX8

793件の閲覧回数
mytemp
Contributor I

Hello,

Our team has recently used The i. MX 8M Mini Quad is designed with LPDDR4 and eMMC5.1. When we tried to download the program to EMMC using UUU, we encountered a problem, and after executing the download command, it stopped at the following interface, and no matter how long we waited, there was no change.

D:\Tools\uuu>uuu -b emmc_all flash.bin rootfs.sdcard
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.141-0-gde317f5

Success 0    Failure 0


1:33     1/ 1 [=================100%=================] SDP: boot -f flash.bin -scanlimited 0x800000

 

After using the uuu -lsusb command, I get the following result

D:\Tools\uuu>uuu -lsusb
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.141-0-gde317f5

Connected Known USB Devices
        Path     Chip    Pro     Vid     Pid     BcdVersion
        ==================================================
        1:33     MX8MM   SDP:    0x1FC9 0x0134   0x0101

What is the reason for this?

 

After executing the download command, the information output from uart2

U-Boot SPL 2018.03-00924-g654088c-dirty (Jun 05 2022 - 20:04:16 -0700)
power_pca9450_init
Can't find PMIC:PCA9450
DRAM PHY training for 2400MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training FAILED
DRAM PHY training for 1336MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training FAILED
DRAM PHY training for 2400MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training FAILED
Normal Boot
Trying to boot from USB SDP

Because the UART4 interface was not used when the hardware was originally designed, it is not possible to obtain information from the UART4 at present.

ラベル(1)
0 件の賞賛
返信
1 返信

750件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信