Hi,
I use LAN8720A and RMII connection to IMX6Q and it works well in kernel 3.10.35,but it does't work in u-boot-2009.08.
when I ping my host,it replies as follows:
MX6Q SABRESD U-Boot > ping 192.168.2.101
ping failed; host 192.168.2.101 is not alive
MX6Q SABRESD U-Boot > ping 192.168.2.101
fec_mii_phy_init: info->phy_addr=0x0
fec_init: info->phy_addr=0x0
FEC: Link is Up 782d
Using FEC0 device
ping failed; host 192.168.2.101 is not alive
MX6Q SABRESD U-Boot > mii device
MII devices: 'FEC0'
Current device: 'FEC0'
MX6Q SABRESD U-Boot > mii dump
Error reading from the PHY addr=00 reg=00
I can't read or write registers by mii read or mii write,it also replies
Error reading from the PHY addr=00 reg=00
My env variables are as follows:
"netdev=eth0\0" \
"ethprime=FEC0\0" \
"uboot=u-boot.bin\0" \
"kernel=uImage\0" \
"ethaddr=1E:ED:19:27:1A:B3\0" \
"nfsroot=/home/van/nfsroot\0" \
"bootargs_base=setenv bootargs console=ttymxc0,115200\0"\
"bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs "\
"ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp\0"\
"bootcmd_net=run bootargs_base bootargs_nfs; " \
"tftpboot ${loadaddr} ${kernel}; bootm\0" \
"bootargs_mmc=setenv bootargs ${bootargs} ip=none " \
"root=/dev/mmcblk0p1 rootwait video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666 ldb=sep0\0" \
"bootcmd_mmc=run bootargs_base bootargs_mmc; " \
"mmc dev 2; " \
"mmc read ${loadaddr} 0x800 0x2000; bootm\0" \
"bootcmd=run bootcmd_mmc\0" \
"update_uboot=tftpboot ${loadaddr} u-boot.bin; sf probe 1; sf erase 0 0x80000; sf write ${loadaddr} 0 0x80000\0" \
"splashimage=0x30000000\0" \
"splashpos=m,m\0" \
"lvds_num=1\0"
Seen below for my schematic diagram:
and the enet_pads table is as follows:
iomux_v3_cfg_t enet_pads[] = {
#ifdef CONFIG_ENET_RMII
/* ENET (10/100Mbps enet interface)*/
MX6Q_PAD_ENET_MDIO__ENET_MDIO,
MX6Q_PAD_ENET_MDC__ENET_MDC,
MX6Q_PAD_ENET_CRS_DV__ENET_RX_EN,
MX6Q_PAD_ENET_RX_ER__ENET_RX_ER,
MX6Q_PAD_ENET_TX_EN__ENET_TX_EN,
MX6Q_PAD_ENET_RXD0__ENET_RDATA_0,
MX6Q_PAD_ENET_RXD1__ENET_RDATA_1,
MX6Q_PAD_ENET_TXD0__ENET_TDATA_0,
MX6Q_PAD_ENET_TXD1__ENET_TDATA_1,
MX6Q_PAD_GPIO_16__ENET_ANATOP_ETHERNET_REF_OUT,
MX6Q_PAD_ENET_REF_CLK__GPIO_1_23, /* reset phy */
#endif
#define CONFIG_ENET_RMII
#define CONFIG_FEC0_IOBASE ENET_BASE_ADDR
#define CONFIG_FEC0_PINMUX -1
#define CONFIG_FEC0_MIIBASE -1
#define CONFIG_GET_FEC_MAC_ADDR_FROM_IIM
#define CONFIG_MXC_FEC
#define CONFIG_FEC0_PHY_ADDR 0xFF
#define CONFIG_DISCOVER_PHY
#define CONFIG_ETH_PRIME
#define CONFIG_RMII
#define CONFIG_CMD_MII
#define CONFIG_CMD_DHCP
#define CONFIG_CMD_PING
#define CONFIG_IPADDR 192.168.2.103
#define CONFIG_SERVERIP 192.168.2.105
and the reset function is :
gpio_direction_output(FEC_PHY_RESET, 0);
udelay(5000);
gpio_set_value(FEC_PHY_RESET, 1);
/* Set GPIO_16 output for RMII reference clock
* For MX6 GPR1 bit21 meaning:
* Bit21: 1 - GPIO_16 pad output
* 0 - GPIO_16 pad input
* Use interal clock, set GPIO_16 output, and
* then force input(set SION)
* Use exteral clock, set GPIO_16 input, and
* don't set SION bit.
*/
mxc_iomux_set_gpr_register(1, 21, 1, 1);
I can measure 50MHZ waveform on GPIO_16.The default PHY is for AR8031,how can modify the codes for LAN8720A in u-boot-2009.08?Is there any patches for this?