Problem with lcd display after booting imx53qsb from sd card

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem with lcd display after booting imx53qsb from sd card

1,543 次查看
onattanriover
Contributor I

I have installed U-boot, the linux kernel and root file system on my sd card from which I intend to boot my imx53qsb. It boots well, but after the boot process I don't get a proper image on the lcd display. Instead, vertical multicolored lines appear on the display and the terminal window on my PC gets filled with random letters. Here are the parameters that I set before the boot process:

MX53-LOCO U-Boot > setenv bootargs_base 'setenv bootargs console=ttymxc0,115200'

MX53-LOCO U-Boot> setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/sdb1 rootwait rw video=mxcdi1fb:BGR24, XGA di1_primary tve'

MX53-LOCO U-Boot> setenv bootcmd_mmc 'run bootargs_base bootargs_mmc;mmc read 0 ${loadaddr} 0x800 0x1800;bootm'

MX53-LOCO U-Boot> setenv bootcmd 'run bootcmd_mmc'

MX53-LOCO U-Boot> saveenv

MX53-LOCO U-Boot> run bootcmd

Does anyone have any idea how I can fix it? Your help will be appreciated.

标签 (3)
0 项奖励
回复
3 回复数

1,294 次查看
Yuri
NXP Employee
NXP Employee

> ... the terminal window on my PC gets filled with random letters.

Is it possible to catch at least first reasonable letters when booting / uncompressing kernel ?

1,294 次查看
Yuri
NXP Employee
NXP Employee

> ... root=/dev/sdb1 ...

Is this correct ?

I expect somewhat as :

root=/dev/mmcblk0p1

1,294 次查看
onattanriover
Contributor I

I've tried both of them and the result is the same.

0 项奖励
回复