Problem with iMX6UL flexcan stuck in Bus off state

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with iMX6UL flexcan stuck in Bus off state

1,057件の閲覧回数
sivakumar_mariy
Contributor I

when I made the miss wire connection of CAN bus the CAN went to bus off state and it never recovers from it. it was recovered only after power cycle. I was tried with both manual and Auto recovery settings in control register

ラベル(3)
タグ(2)
0 件の賞賛
返信
1 返信

991件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi sivakumar 

first may be recommended to verify the physical configuration on custom board as

flexcan is very sensitive to it.
The flexcan transmitter may not send any data because the receiver was wrongly
detecting that the bus was currently in use.
The STBY signal may be always on, keeping in low power mode the flexcan module,
therefore, it does not listen to anything. 

Flexcan module can be tested with unit tests:

doc\can\test - imx-test - i.MX Driver Test Application Software 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信