Problem with iMX6UL flexcan stuck in Bus off state

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with iMX6UL flexcan stuck in Bus off state

1,119 Views
sivakumar_mariy
Contributor I

when I made the miss wire connection of CAN bus the CAN went to bus off state and it never recovers from it. it was recovered only after power cycle. I was tried with both manual and Auto recovery settings in control register

Labels (3)
0 Kudos
Reply
1 Reply

1,053 Views
igorpadykov
NXP Employee
NXP Employee

Hi sivakumar 

first may be recommended to verify the physical configuration on custom board as

flexcan is very sensitive to it.
The flexcan transmitter may not send any data because the receiver was wrongly
detecting that the bus was currently in use.
The STBY signal may be always on, keeping in low power mode the flexcan module,
therefore, it does not listen to anything. 

Flexcan module can be tested with unit tests:

doc\can\test - imx-test - i.MX Driver Test Application Software 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply