Problem with burn bootloader into eMMC with UUU on IMX6UL-EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with burn bootloader into eMMC with UUU on IMX6UL-EVK

Jump to solution
2,752 Views
kr90911
Contributor III

Hi all,
I want to boot from eMMC,but I got error when I burn eMMC whith UUU on IMX6ULEVK.
The error messages as follow:

UUU_PowerShell_log.JPG

Debug log as follow:

U-Boot 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df (Apr 11 2019 - 13:47:37 +0000)
CPU: Freescale i.MX6UL rev1.0 528 MHz (running at 396 MHz)
CPU: Industrial temperature grade (-40C to 105C) at 39C
Reset cause: POR
Model: Freescale i.MX6 UltraLite 14x14 EVK Board
Board: MX6UL 14x14 EVK
DRAM: 512 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment
Failed (-5)
Display: TFT43AB (480x272)
Video: 480x272x24
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc1 is current device
Net:
Warning: ethernet@020b4000 using MAC address from ROM
eth1: ethernet@020b4000 [PRIME]
Warning: ethernet@02188000 using MAC address from ROM
, eth0: ethernet@02188000
Fastboot: Normal
Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else bootz ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; fi;
Hit any key to stop autoboot: 0
## Checking Image at 86800000 ...
Unknown image format!
Run fastboot ...
flash target is MMC:1
switch to partitions #0, OK
mmc1 is current device
Starting download of 16776232 bytes
..........................................................................
.....................................................
downloading of 16776232 bytes finished
writing to partition 'all'
sparse flash target is mmc:1
writing to partition 'all' for sparse, buffer size 16776232
Flashing sparse image at offset 0
Flashing Sparse Image
........ wrote 16776192 bytes to 'all'
Starting download of 16776244 bytes
..........................................................................
.....................................................
downloading of 16776244 bytes finished
writing to partition 'all'
sparse flash target is mmc:1
writing to partition 'all' for sparse, buffer size 16776244
Flashing sparse image at offset 0
Flashing Sparse Image
........ wrote 16776192 bytes to 'all'
Starting download of 16776244 bytes
..........................................................................
.....................................................

..........................................................................
.....................................................
downloading of 16776244 bytes finished
writing to partition 'all'
sparse flash target is mmc:1
writing to partition 'all' for sparse, buffer size 16776244
Flashing sparse image at offset 0
Flashing Sparse Image
........ wrote 16776192 bytes to 'all'
Starting download of 16776244 bytes
..........................................................................
.....................................................
downloading of 16776244 bytes finished
writing to partition 'all'
sparse flash target is mmc:1
writing to partition 'all' for sparse, buffer size 16776244
Flashing sparse image at offset 0
Flashing Sparse Image
........ wrote 16776192 bytes to 'all'
Starting download of 8451124 bytes
................................................................
downloading of 8451124 bytes finished
writing to partition 'all'
sparse flash target is mmc:1
writing to partition 'all' for sparse, buffer size 8451124
Flashing sparse image at offset 0
Flashing Sparse Image
........ wrote 8451072 bytes to 'all'
Starting download of 609280 bytes
....
downloading of 609280 bytes finished
writing to partition 'bootloader'
support sparse flash partition for bootloader
Initializing 'bootloader'
switch to partitions #0, OK
mmc1 is current device
Writing 'bootloader'
MMC write: dev # 1, block # 2, count 1190 ... 1190 blocks written: OK
Writing 'bootloader' DONE!
PARTITION_CONFIG only exists on eMMC‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Hope you can give me some suggestions,

thanks.

Labels (1)
Tags (4)
0 Kudos
Reply
1 Solution
2,489 Views
igorpadykov
NXP Employee
NXP Employee

had you soldered emmc, as there is no emmc on EVK.

Best regards
igor

View solution in original post

3 Replies
2,489 Views
igorpadykov
NXP Employee
NXP Employee

Hi west

one can recheck i.MX6UL EVK emmc usage with sect.2.6 eMMC
i.MX 6UltraLite EVK Board Hardware User's Guide

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,489 Views
kr90911
Contributor III

Hi igor,

Thanks for your response.

I read  i.MX 6UltraLite EVK Board Hardware User's Guide and set pin like follow:

P_20200121_090641.jpg.jpg

Nothing show on debug screen.

Have any suggestions?

Thanks,

west

0 Kudos
Reply
2,490 Views
igorpadykov
NXP Employee
NXP Employee

had you soldered emmc, as there is no emmc on EVK.

Best regards
igor