Problem with NTSC video

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with NTSC video

3,850 Views
jotes
Contributor IV

Hello!

I'm trying to integrate the TW9910 and SABRE LITE, and have a problem with the NTSC video format. The video seems to be floating in time: for about 16 seconds it is correct, then for about 16 seconds it looks like the fields are mixed (but it is only seen on the moving elements, the background looks fine), and so on. Please check the images attached - both cases are illustrated.

The versions of software are: GStreamer-imx Plugins 0.11.1, Linux 3.14.38 (linux-imx6-boundary-imx_3.14.38_6qp_beta-cec). I'm using following command:

gst-launch-1.0 -v imxv4l2videosrc num-buffers=-1 device=/dev/video0 ! imxipuvideotransform ! imxipuvideosink window-width=720 window-height=480 sync=true

I have no idea what causes this strange effect. Could you please help me?

Labels (3)
0 Kudos
Reply
5 Replies

2,900 Views
donggyulee
Contributor I

Hi,

did you solve this problem?

i have a same problem.

please let me know

thank you

0 Kudos
Reply

2,900 Views
jotes
Contributor IV

No, the problem is still unsolved.

0 Kudos
Reply

2,900 Views
joanxie
NXP TechSupport
NXP TechSupport

did you try to use the unit test? if still has this issue, pls upload your log file.

0 Kudos
Reply

2,900 Views
jotes
Contributor IV

joanxie​ ?

0 Kudos
Reply

2,900 Views
jotes
Contributor IV

When I use unit_tests, the effect is still the same. But which log file did you mean? The test shows only:

# /unit_tests/mxc_v4l2_tvin.out -ow 720 -oh 480

TV decoder chip is tw9910_decoder

VIDIOC_G_FMT failed

driver=mxc_vout, card=DISP4 FG, bus=, version=0x00030e26, capabilities=0x04000002

fmt RGB565: fourcc = 0x50424752

fmt BGR24: fourcc = 0x33524742

fmt RGB24: fourcc = 0x33424752

fmt RGB32: fourcc = 0x34424752

fmt BGR32: fourcc = 0x34524742

fmt NV12: fourcc = 0x3231564e

fmt UYVY: fourcc = 0x59565955

fmt YUYV: fourcc = 0x56595559

fmt YUV422 planar: fourcc = 0x50323234

fmt YUV444: fourcc = 0x34343459

fmt YUV420: fourcc = 0x32315559

fmt YVU420: fourcc = 0x32315659

fmt TILED NV12P: fourcc = 0x50564e54

fmt TILED NV12F: fourcc = 0x46564e54

fmt YUV444 planar: fourcc = 0x50343434

start time = 177 s, 150539 us

0 Kudos
Reply