A. Screen settings
My screen setting is HDMI, 1920x1080, the u-boot settings are:
set hdmi_1080 'video=mxcdi0fb:RGB24,1920x1080MR-16@60 hdmi di0_primary'
set bootargs_base 'setenv bootargs console=ttymxc0,115200 hdmi_1080'
B. Test video file of mpeg2 video :
ftp://alright-2:alright1689@alright.com.tw, enter the folder i.MX/test_video, 908001.vob, 908002.vob
C. Test environment :
a. lucid image from L2.6.35_11.01.00_ER_images_MX5X.tar.gz, rootfs.tar.bz2
b. linux kernel 2.6.35 built from LTIB L2.6.35_11.01.00_ER_source_bundle
c. linux kernel 2.6.35 built from LTIB L2.6.35_11.09.01_ER_source_bundle.tar.gz
D. Test procedure :
gplay [test video filename]
E. Test result :
a. (lucid image) : The video files can be playback, however, the screen will turn to black sometime with IPU error message prompted. After a few seconds, the video will appear on screen again.
mxc_ipu mxc_ipu: IPU Error - IPU_INT_STAT_10 = 0x00080000
b. & c. (built from ltib) : The video files can not be playback normally, with VDI split not support message, and the frame rate only has fps:8, no video on screen at all.
video4linux video16: VDI split has not supported yet.
[Playing ][Vol=01][00:00:01/00:02:53][fps:8]
Is there anybody know how to let these video play normally without screen turn to black ? Thanks.
In additional, the codec I used is IMX_MMCODECS_11.09 from "http://www.freescale.com/webapp/Download?colCode=IMX53_11_09_LINUX_MMCODECS"