We developed the board using imx6 solo and Linkstreet (Ethernet switch) of Marvell.
However, the board has a problem which an ENET_EIR [GRA] interrupt occurs and transmitting stops, when traffic increases.
.
The occurrence of cause of GRA interrupt is mention to the reference manual(23.4.9.4.1 Graceful transmit stop (GTS)),
but that doesn't apply to any of them.
I think that the Marvell tag added to the header caused problem.
Then, please let me know about following,
- When it stops by GRA interrup, is there any method of resume transmission?
The method of clearing ENET_TCR [GTS] was not effective.
-I think that the Marvell tag is misrecognition to be pause frame.
Is there any method of disable pause frame?