Problem of ENET_EIR [GRA] interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem of ENET_EIR [GRA] interrupt

991 Views
t_kaz
Contributor I

We developed the board using imx6 solo and Linkstreet (Ethernet switch) of Marvell.

However, the board has a problem which an ENET_EIR [GRA] interrupt occurs and transmitting stops, when traffic increases.

.

The occurrence of cause of GRA interrupt is mention to the reference manual(23.4.9.4.1 Graceful transmit stop (GTS)),

but that doesn't apply to any of them.

I think that the Marvell tag added to the header caused problem.

Then, please let me know about following,

- When it stops by GRA interrup, is there any method of resume transmission?

The method of clearing ENET_TCR [GTS] was not effective.

-I think that the Marvell tag is misrecognition to be pause frame.

Is there any method of disable pause frame?

Labels (1)
0 Kudos
Reply
4 Replies

770 Views
YixingKong
Senior Contributor IV

t-Kaz

Could you please rspond to Jozef's questions as soon as possible?

Thanks,

Yixing

0 Kudos
Reply

770 Views
cyborgnegotiato
Senior Contributor II

Hi,

Did you try disable flow control? ENET_RCR[FCE].

How you clear the ENET_TCR[GTS]?

What is state of ENET_TCR[RFC_PAUSE] in your unpleasant situation?

Thanks,

Jozef

0 Kudos
Reply

770 Views
YixingKong
Senior Contributor IV

t-Kaz

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow to resolved the issue, can we close the discussion? If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
Reply

769 Views
t_kaz
Contributor I

Thank you for your reply,

I'm still stuck with the issue, Please advice me.

0 Kudos
Reply