Problem in Qt5 in MCIMX6UL-EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem in Qt5 in MCIMX6UL-EVK

1,014件の閲覧回数
ko-hey
Senior Contributor II

Hi all

My customer is using following environment and have some problem.

So let me confirm about Qt5 support in MCIMX6UL-EVK.

・MCIMX6UL-EVK

     Branch : imx-3.14.38-6UL_ga, imx_4.1.15_1.0.0_ga

     Machine : imx6ulevk

     Backend : X11

     Project : fsl-image-qt5 

My customer want to try Qt5 app and touch the icon which is shown on the screen.

But it didn't response.

I think it caused i.MX6UL doesn't have GPU.

Is it correct ?

Ko-hey

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 返信

840件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Ko-hey,

Yes, you are right. There is no internal GPU on MCIMX6UL. If you need high Operational Capability on 3D, here I recommend you to use the other i.mx6 series products with GPU. Hope this can help you.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信