Dears,
I've installed https://community.nxp.com/docs/DOC-330147 on imx6qp and want to have a print on my HDMI screen during booting. I'm able to have print output on host PC onto console output. Is it possible to configure it such a way that to have 'print' of booting onto attached screen. for now I have have login GUI .
Thanks.
Hi Erik,
We do use HDMI output by default on a mx6cubox board if it detects that HDMI cable is connected.
You can get the details at git.denx.de Git - u-boot.git/blob - include/configs/mx6cuboxi.h
but the relevant logic is:
"if hdmidet; then " \
"usb start; " \
"setenv stdin serial,usbkbd; "\
"setenv stdout serial,vga; " \
"setenv stderr serial,vga; " \
"else " \
"setenv stdin serial; " \
"setenv stdout serial; " \
"setenv stderr serial; " \
"fi;"
Regards,
Fabio Estevam
Is it possible to modify it within u-boot console?
> setenv stdin serial,usbkbd
> setenv stdout serial,vga
> setenv stderr serial,vga
> saveenv
but I when setenv stdout vga then uboot console freeze. Have you ever try it to set from console?
What you mean by enabling U-boot support?
I do:
setenv mmcargs $mmcargs video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 saveenv
then
> setenv stdin serial,usbkbd
> setenv stdout serial,vga
> setenv stderr serial,vga
> saveen
Do you mean another way to make sure HDMI support is enabled?
Or maybe I misunderstood your goal: it seems you want to get the kernel log printed into HDMI.
If this is the case you need to pass: console=tty0 prior to console=ttymxc0,115200 into your kernel command line.
for u-boot
$ wget –c http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/snapshot/uboot-imx-rel_imx_4.1.15_2.0.0_ga.t...
$ tar -xf uboot-imx-rel_imx_4.1.15_2.0.0_ga.tar.gz
$ cd uboot-imx-rel_imx_4.1.15_2.0.0_ga
$ make $mx6qpsabreauto_config
$ make
no other than this config I did.
I'd like to have u-boot from within HDMI console (setenv stdout vga just hangs)
# Enabling HDMI comsole
setenv panel HDMI
setenv stdout serial,vga
setenv stderr serial,vga
saveenv# To tell U-Boot to accept console input from a USB keyboard, run the following commands:
setenv stdin serial,usbkbd
saveenv# To make U-Boot detect the USB keyboard on boot, run the following commands:
setenv preboot "usb start"
saveenv
as you asked: I am asking if you have enabled HDMI support inside U-Boot,
I think that's what I'm missing...
How can I enable HDMI support inside U-Boot?
Have you tried to download the associated documentation package -
Embedded Linux for i.MX Applications Processors|NXP
From memory the default output is LVDS, but the QSG or similar documentation explains how to switch to the HDMI output.
Regards
Ross
Yes, I did. I got the documentation package for fsl-yocto-L4.1.15_2.0.0-ga. Can please point me where can I find more about?
BTW I switch the output to HDMI
setenv mmcargs 'setenv bootargs console=ttymxc0,115200 root=/dev/mmcblk2p2 rootwait rw video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24'
Actually I've got output of GUI but no booting info which I can onky see on host console of PC via UART (console=ttymxc3)
I found this How to config the hdmi with uboot
Hopefully this helps, I also tried a quick google for outputting Linux console messages on HDMI, threw up a lot of hits, so might be worth a look there also, if above doesn't help.
Ross