Trying to use preview property in mfw_v4lsrc.
I have gstreamer0.10.36 and related codecs with freescale plugin gst-fsl-plugins2.0.3 and IMX_MMCODECS_11_09 for imx53.
When i fire the following gstreamer pipeline. I do get the preview as i expected but when i kill the pipeline the preview still remains and does not destroy as expected.
gst-launch -e -v --gst-debug-level=3 \
mfw_v4lsrc capture-mode=3 capture-width=640 capture-height=480 sensor-height=640 sensor-width=480 preview=true preview-top=100 preview-left=50 preview-width=200 preview-height=200 ! \
mfw_ipucsc ! \
"video/x-raw-yuv,format=(fourcc)I420,width=$WIDTH,height=$HEIGHT,framerate=(fraction)90000/3000" ! \
queue max-size-buffers=1000 ! \
mfw_vpuencoder codec-type=2 ! \
queue max-size-buffers=1000 ! \
rtph264pay config-interval=5 pt=113 mtu=1444 ! \
udpsink port=5000
One more thing I have used same pipeline with bg=true as below, able to see preview but as soon as my another pipeling for the sink runs but videos gets merge togather but i can able to kill the preview as well as other video.
gst-launch -e -v --gst-debug-level=3 \
mfw_v4lsrc capture-mode=3 capture-width=640 capture-height=480 sensor-height=640 sensor-width=480 preview=true preview-top=100 preview-left=50 preview-width=200 preview-height=200 bg=true ! \
mfw_ipucsc ! \
"video/x-raw-yuv,format=(fourcc)I420,width=$WIDTH,height=$HEIGHT,framerate=(fraction)90000/3000" ! \
queue max-size-buffers=1000 ! \
mfw_vpuencoder codec-type=2 ! \
queue max-size-buffers=1000 ! \
rtph264pay config-interval=5 pt=113 mtu=1444 ! \
udpsink port=5000
I cannot use mfw_v4lsink and create another pipeline for the preview mechanism as i am using mfw_v4lsrc and mfw_v4lsink at the same time for different purpose. So it will be 2 videos running in same display. Kind of PIP. I dont want to use mfw_isink as it is slow.
I have searched the community and no one has encounter similar problem.
Thanks,
Tarak Patel