Preempt-RT

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Preempt-RT

跳至解决方案
1,506 次查看
ChrisChang1234
Contributor III

1. I'm looking for the patches that 'Only' enables the "Preemt-RT" feature.

    refer to 

    https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/Enable-Linux-RT-PREEMPT-on-i-MX8M-Products/t...

But I don't know how get the patches for kernel 5.10.72 and 6.1.1x.

 

2.  Per customer's request, we have to replace the original rootfs with other version.

    If we do so, will the "Preempt RT" feature keep available?

    (in other words, the preempt rt patches impact kernel image only or also including the roots?) 

   

    

标签 (1)
0 项奖励
回复
1 解答
1,479 次查看
joanxie
NXP TechSupport
NXP TechSupport

1)the owner doesn't update to the latest bsp version, maybe customer needs to change the new bsp source code according to the patches based on 4.1478

2) refer to the readme, these patches are for kernel, customer just needs to change the kernel image, they just replace the new kernel image only

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,471 次查看
ChrisChang1234
Contributor III

Got it, thanks

0 项奖励
回复
1,480 次查看
joanxie
NXP TechSupport
NXP TechSupport

1)the owner doesn't update to the latest bsp version, maybe customer needs to change the new bsp source code according to the patches based on 4.1478

2) refer to the readme, these patches are for kernel, customer just needs to change the kernel image, they just replace the new kernel image only

0 项奖励
回复