Hi Sir ,
Could you please share me the android prebuilt image for IMX6 sabresd board (evaluation kit)
解決済! 解決策の投稿を見る。
Please use Freescale web to download the packages.
The following is Summary page link :
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX6_SW
The demo image for SABRE Platform and SABRE Board for Smart Devices :
Documentation :
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi
Sachu
Go to Run-time software, and select required BSP image.
Thanks
Saurabh
Hai sourabh ,
thanks for your response
could you please help me to flash the image to SD card
Hi
Sachu
You need to use mfgtool.
Use SD card profile from ucl2.xml,
make a code change in cfg.ini file and replace eMMC with SD card profile from ucl2.xml
Thanks
Saurabh
Hi
i would like to use dd utility for flashing the image means I have an SD card so using dd utility i can copy the images easily,but what is the problem iam facing means before using dd utility i need to create partistion.
please tell how can create partision
sudo fdisk /dev/sdb
Download the U-Boot image:
# sudo dd if=u-boot.imx of=/dev/sdx bs=1K seek=1; sync
Download the boot image:
# sudo dd if=boot.img of=/dev/sdx1; sync
Download the Android system root image:
# sudo dd if=system.img of=/dev/sdx5; sync
Download the Android recovery image:
# sudo dd if=recovery.img ox2; syncf=/dev/sd
Please use Freescale web to download the packages.
The following is Summary page link :
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX6_SW
The demo image for SABRE Platform and SABRE Board for Smart Devices :
Documentation :
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
could you please give me the mfgtools.tar.gz. for android_KK4.4.3_2.0.0-ga_core_image
Thanks for your response..
I download the android_KK4.4.3_2.0.0-ga_core_image_6qsabresd.tar.gz file .I need to flash the Image by using SD card
could you please help me how can create partion.
from the Document section I couldnt understand how to create partion and how to flash the images
please help me