Powering imx233 only by internal linear regulator

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Powering imx233 only by internal linear regulator

跳至解决方案
1,379 次查看
francescochino
Contributor I

Hi,

I need some example of imx-bootlet file to boot the imx233 using only the internal linear power supply. Is this code available? Could I send my code that needs to checked?

Thank you in advance for your support.

Regards

Francesco

标签 (1)
0 项奖励
回复
1 解答
1,238 次查看
igorpadykov
NXP Employee
NXP Employee

HI Francesco

one can check 5V only mode, it is well tested on i.MX28 EVK

Updates and Patches (9)

Linux patch for i.MX28 SDK 2010.12 to add the most robust support

possible for a VDD5V or DCDC_BATT only configuration.

i.MX28 Evaluation Kit|Freescale

processor works from LDOs until hw_power_Enable4p2DcdcInput()

in hw_power.c imx-bootlets.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,238 次查看
francescochino
Contributor I

Hi Igor,

we have halfed the processor speed and now the board boots correctly.

Thank you for your support

My Best Regards

Francesco

0 项奖励
回复
1,239 次查看
igorpadykov
NXP Employee
NXP Employee

HI Francesco

one can check 5V only mode, it is well tested on i.MX28 EVK

Updates and Patches (9)

Linux patch for i.MX28 SDK 2010.12 to add the most robust support

possible for a VDD5V or DCDC_BATT only configuration.

i.MX28 Evaluation Kit|Freescale

processor works from LDOs until hw_power_Enable4p2DcdcInput()

in hw_power.c imx-bootlets.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复