Power measurement in SabreSD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Power measurement in SabreSD

944件の閲覧回数
senthilkumarcha
Contributor III

Hi, 

I am measuring power in sabreSD board with kernel version 4.9.11. For Kernel version 4.1.15 the current consumption is close to the values given in the reference document https://www.nxp.com/docs/en/application-note/AN5383.pdf . For kernel version 4.9.11, the current consumption is little higher.

The table below shows the differences.

Linux-4.1.15

(mA)

Linux-4.9.11

(mA)

VDD_SOC – R241.422.25
VDD_ARM – R200.4670.619
VDDA_1P8 - L520.50.5

Is there reference document for power measurement with kernel version 4.9.11 ?

Do we need any power management steps for reducing power in version 4.9.11 ?

Thanks in Advance,

C.Senthilkumar

ラベル(3)
0 件の賞賛
返信
1 返信

834件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Senthilkumar

I am not aware of power measurements with kernel version 4.9.11,

but document describes why power data may vary, please check

sect.3.2.1. ODT settings, sect.3.4. Temperature measurements

AN5383 i.MX 7DS Power Consumption Measurement

https://www.nxp.com/docs/en/application-note/AN5383.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信