Power management with GPU not working in WinCE7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Power management with GPU not working in WinCE7

1,358 Views
Sowmya1z
Contributor II

Dear All,

  I am working in freescale's imx6q SDP platform. The target uses wince7 OS.Following issue i am facing:

When i give suspend, i am getting the following exception:

VMProcessPageFault Error: Page fault occurred while in power handler! Address = 0x00000000

TID:00DB0006 Exception 'Prefetch Abort' (0x3): Thread-Id=00db0006(pth=c0808790), Proc-Id=00400002(pprc=83b3f5e0) 'NK.EXE', VM-active=045a0052(pprc=c087b75c) 'servicesd.exe'

TID:00DB0006 PC=00000000(???+0x00000000) RA=eee76874(libgalcore.dll+0x00006874) SP=cca4f7c0, BVA=00000000.

The system is resuming after this exception. But the second time when i give suspend, the system is going to suspend, but not able to resume.

When the GPU driver is removed, the suspend and resume is happening without any exceptions.

Please help me to solve this issue.

Thanks and Regards,

Sowmya


Labels (1)
Tags (4)
0 Kudos
Reply
1 Reply

1,022 Views
karina_valencia
NXP Apps Support
NXP Apps Support

Deactivated user can you  help  on this case?

0 Kudos
Reply