Power group in pinmux conflict

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Power group in pinmux conflict

Jump to solution
1,977 Views
matt67
Contributor III

Hi there,

We are using pintool to assign pad of an i.mx8mm and dealing with 1.8 and 3.3 voltage domains.

We uses by example GPIO1_IO10 PAD as GPIO1_IO10  in powergroup NVCC_GPIO1 suplied in 1.8V (we wan this GPIO in 1.8V)

We also use the pad ENET_RD2 in alternate GPIO1_IO28 (we wan this GPIO in 3.3V) supplied by NVCC_ENET in 3.3V and a warning is appearing about a potential conflict, I cant figure out clearly in the Reference Manual if this is a real issue or not.

Is it a mistake to assign the pad as shown ?

pinmux.png

error.png

Thank you,

0 Kudos
Reply
1 Solution
1,864 Views
igorpadykov
NXP Employee
NXP Employee

Hi matt67

there is no conflict and ENET_RD2 can be used with NVCC_ENET at 3.3V ,

one can look at Table 64. i.MX 8M Mini 14 x 14 mm functional contact assignments

"Power group" column :

i.MX 8M Mini Applications Processor Datasheet for Consumer Products

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,865 Views
igorpadykov
NXP Employee
NXP Employee

Hi matt67

there is no conflict and ENET_RD2 can be used with NVCC_ENET at 3.3V ,

one can look at Table 64. i.MX 8M Mini 14 x 14 mm functional contact assignments

"Power group" column :

i.MX 8M Mini Applications Processor Datasheet for Consumer Products

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,864 Views
matt67
Contributor III

Thanks for answering

0 Kudos
Reply