I am Porting uboot 2017.03 to myown board (use i.Mx6SOLO). The board work well with uboot 2015.04, but when I ported the uboot 2017.03 to the board I meet the follow issue:
My board don't use the PMIC moduel, so I edit the code about "pfuze100" . The attachment is the changes I do from the YOCTO "imx-yocto-L4.9.88_2.0.0".
Some esle can help me find the problem??
Hi Wuxiumxin,
if board is based on nxp evk design I believe these settings
can be left in default state. It is necessary to run ddr test
i.MX6/7 DDR Stress Test Tool V2.90
and change uboot/../mx6ullevk/imximage_lpddr2.cfg with new calibration
coefficients found from test.
Regards
Hi,
I find the problem two days ago. I configure the dtb about the uSDHC and the issue is solved. thanks.