Hi...
I am trying to port camera capture driver from Linux kernel v 3.10.17 [customized - don't have details :smileysad:] to v 4.1.1 [Freescale/linux-fslc at v4.1.1 ยท GitHub].
I am getting errors in ipuv3 related functions. When checked, I could observe that ipuv3 related code has difference in the new kernel.
For example:
fatal error: linux/ipu-v3.h: No such file or directory
Can I get some reference on how to port the ipuv3 code?
Thanks & Regards,
Binoy.
I'm working on MX6 parallel camera support based on the patches from Philipp Zabel. I forward-ported them to 4.1.4, you can find them here LINK. I managed to get OV5642 Parallel Camera working with BD SabreLite and I managed to capture 640x480 picture. I didn't manage to capture a picture in any other resolution yet, this needs more work it seems.
To capture a still picture, compile the code (the sabrelite_defconfig has all the necessary options enabled, so use that to boot) and use this script to obtain an /x.png :
#!/bin/bash
WIDTH=640
HEIGHT=480
FMT=${WIDTH}x${HEIGHT}
media-ctl -l '"ov5642 1-003c":0->"mipi_ipu1_mux":1[1], "/soc/ipu@02400000/port@0":1->"IPU0 SMFC0":0[1]'
media-ctl -l '"IPU0 SMFC0":1->"imx-ipuv3-camera.2":0[1]'
# From camera to ipu1 mux
media-ctl -V '"mipi_ipu1_mux":1[fmt:YUYV2X8/'$FMT']'
# From ipu1 mux to ipu
media-ctl -V '"mipi_ipu1_mux":2[fmt:YUYV2X8/'$FMT']'
# ipu
media-ctl -V '"/soc/ipu@02400000/port@0":1[fmt:YUYV2X8/'$FMT']'
v4l2-ctl -d0 --set-fmt-video=width=${WIDTH},height=${HEIGHT},pixelformat=UYVY
echo "Capturing"
v4l2-ctl -d0 --stream-mmap --stream-to=/x.raw --stream-count=1
echo "Encoding"
convert -size $FMT -depth 16 uyvy:/x.raw /x.png