Porting LCD driver to uboot on imx8ulp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Porting LCD driver to uboot on imx8ulp

2,253 Views
wangrucheng
Contributor I

LCD parameters

static const struct display_timing default_timing = {
    .pixelclock.typ     = 27000000,
    .hactive.typ        = 480,
    .hfront_porch.typ   = 20,
    .hback_porch.typ    = 35,
    .hsync_len.typ      = 4,

    .vactive.typ        = 800,
    .vfront_porch.typ   = 10,
    .vback_porch.typ    = 20,
    .vsync_len.typ      = 4,
};
controller:st7701s
mipi lane:2
format: RGB888
mode:MIPI_DSI_MODE_VIDEO | MIPI_DSI_MODE_LPM | MIPI_DSI_MODE_VIDEO_BURST
    plat->lanes = priv->lanes;
    plat->format = MIPI_DSI_FMT_RGB888;
    plat->mode_flags = MIPI_DSI_MODE_VIDEO | MIPI_DSI_MODE_LPM | MIPI_DSI_MODE_VIDEO_BURST;
 
The same logic can run normally in the kernel, but it does not run properly in the uboot stage.

Can you give me some advice?

Thanks

 

0 Kudos
Reply
5 Replies

2,227 Views
brian14
NXP TechSupport
NXP TechSupport

Hi @wangrucheng

Thank you for contacting NXP Support.

This problem could be caused due to a difference in device tree used in both stages, U-boot and Kernel.
Please confirm that you are using the same device tree.

Have a great day!

0 Kudos
Reply

2,165 Views
wangrucheng
Contributor I

Hi @brian14

Have you ever checked this issue? I am currently stuck here and the deadline is very close.

Thanks!

0 Kudos
Reply

2,223 Views
wangrucheng
Contributor I

I am sure there is nothing wrong with the device tree I am using, because hx8394f panel can display the NXP log during the uboot startup phase.but my panel can't.

I uploaded device tree and panel code. 

0 Kudos
Reply

2,153 Views
brian14
NXP TechSupport
NXP TechSupport

Hi @wangrucheng

Could you please clarify your last reply?
In your first question you are saying that the problem is on uboot stage. However, in your last reply you are saying that your panel is working on uboot stage.

Also, I can't see your device tree or panel code. Could you please reupload your files?

Have a great day!

0 Kudos
Reply

2,121 Views
wangrucheng
Contributor I

I used a screen with ST7701S as the controller. Currently, the kernel can display the image normally, but when I porting it to uboot, I found that the NXP logo could not be displayed normally.

What I can confirm is that there is no problem with the device tree and there is no problem with the screen initialization code.

The attachment contains uboot kernel code and panel spec.

0 Kudos
Reply