Porting IMX477 for IMX8MP Isp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Porting IMX477 for IMX8MP Isp

3,549件の閲覧回数
CanberkOzbey
Contributor I

Hello All

I am working on porting an IMX477 camera driver to the IMX8MP EDM-g-WB board of technexion.I am following the i.MX 8M Plus Camera and Display Guide, section 2 Camera Sensor Porting Guide and 8MP ISP New Camera Porting Guide.

When i try to use gstreamer command i get the following error.

root@edm-g-imx8mp:~# gst-launch-1.0 -vvv v4l2src device=/dev/video0 num-buffers=1 \! "video/x-bayer,width=1920,height=1080,framerate=(fraction)25/1,format=(string)bggr" \! bayer2rgb ! pngenc ! filesink location=test.png
[ 2872.204035] enter isp_mi_stop
Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Internal data stream error.
Additional debug info:
../git/libs/gst/base/gstbasesrc.c(3127): gst_base_src_loop (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0:
streaming stopped, reason not-negotiated (-4)
Execution ended after 0:00:00.717251750
Setting pipeline to NULL ...
Freeing pipeline ...

When try to use v4l2 to get a photo i get this as output

root@edm-g-imx8mp:~# v4l2-ctl --device /dev/video0 --stream-mmap --stream-to=frame.raw --stream-count=1 [ 3319.179967] ------------[ cut here ]------------
[ 3319.184597] WARNING: CPU: 1 PID: 884 at drivers/media/common/videobuf2/videobuf2-core.c:807 vb2_core_reqbufs+0x138/0x400
[ 3319.195477] Modules linked in: imx477(O) imx8_media_dev(C) vvcam_video(O) vvcam_isp(O) vvcam_dwe(O) algif_skcipher fsl_jr_uio caam_jr caamkeyblob_desc caamhash_desc caamalg_desc crypto_engine rng_core authenc libdes crct10dif_ce snd_soc_imx_hdmi wlan(O) snd_soc_fsl_easrc dw_hdmi_cec snd_soc_fsl_sai snd_soc_fsl_aud2htx flexcan can_dev caam secvio error i2c_gpio [last unloaded: imx8_media_dev]
[ 3319.230214] CPU: 1 PID: 884 Comm: v4l2-ctl Tainted: G WC O 5.15.52+gd6c58d2ff21e #1
[ 3319.238910] Hardware name: TechNexion EDM-G-IMX8MP and WB baseboard (DT)
[ 3319.245608] pstate: 80000005 (Nzcv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[ 3319.252567] pc : vb2_core_reqbufs+0x138/0x400
[ 3319.256923] lr : vb2_core_reqbufs+0x100/0x400
[ 3319.261278] sp : ffff80001b32ba50
[ 3319.264588] x29: ffff80001b32ba50 x28: ffff000004119400 x27: 0000000000000000
[ 3319.271725] x26: 0000000000000000 x25: ffff80001b32bd28 x24: 0000000000000000
[ 3319.278861] x23: ffff000004119508 x22: 0000000000000001 x21: ffff80001b32bd28
[ 3319.285997] x20: 0000000000000000 x19: ffff0000041194a0 x18: 0000000000000000
[ 3319.293133] x17: 0000000000000000 x16: 0000000000000000 x15: 0000ffffc1f7c328
[ 3319.300268] x14: 0000000000000000 x13: 0000000000000000 x12: 0000000000000000
[ 3319.307404] x11: 0000000000000000 x10: 0000000000000000 x9 : 0000000000000000
[ 3319.314540] x8 : ffff000004119548 x7 : 0000000000000000 x6 : 0000000010000000
[ 3319.321676] x5 : 0000000000000000 x4 : 0000000000000000 x3 : 0000000000000001
[ 3319.328811] x2 : ffff80001b32baac x1 : ffff80001b32baa0 x0 : ffff80001b32baa8
[ 3319.335947] Call trace:
[ 3319.338391] vb2_core_reqbufs+0x138/0x400
[ 3319.342399] vb2_reqbufs+0x5c/0x7c
[ 3319.345800] vidioc_reqbufs+0x144/0x200 [vvcam_video]
[ 3319.350854] v4l_reqbufs+0x50/0x6c
[ 3319.354255] __video_do_ioctl+0x178/0x3dc
[ 3319.358262] video_usercopy+0x368/0x6ec
[ 3319.362096] video_ioctl2+0x1c/0x30
[ 3319.365583] v4l2_ioctl+0x44/0x64
[ 3319.368897] __arm64_sys_ioctl+0xac/0xf0
[ 3319.372821] invoke_syscall+0x48/0x114
[ 3319.376570] el0_svc_common.constprop.0+0xd4/0xfc
[ 3319.381275] do_el0_svc+0x2c/0x94
[ 3319.384588] el0_svc+0x28/0x80
[ 3319.387643] el0t_64_sync_handler+0xa8/0x130
[ 3319.391914] el0t_64_sync+0x1a0/0x1a4
[ 3319.395575] ---[ end trace d7a0f9a20adad406 ]---
VIDIOC_REQBUFS returned -1 (Invalid argument)

My Dmesg output

root@edm-g-imx8mp:~# dmesg |grep imx477
[ 45.532556] enter imx477_probe
[ 45.536796] enter imx477_retrieve_capture_properties
[ 45.541962] imx477 1-001a: supply DOVDD not found, using dummy regulator
[ 45.549007] imx477 1-001a: supply DVDD not found, using dummy regulator
[ 45.555806] imx477 1-001a: supply AVDD not found, using dummy regulator
[ 45.562618] enter imx477_regulator_enable
[ 45.566660] enter imx477_set_clk_rate
[ 45.570386] enter imx477_power_on
[ 45.574056] enter imx477_reset
[ 45.631773] enter imx477_read_reg
[ 45.635629] enter imx477_read_reg
[ 45.639498] imx477_probe camera mipi imx477, is found

 

My media-ctl output

root@edm-g-imx8mp:~# media-ctl -p
Media controller API version 5.15.52

Media device information
------------------------
driver vvcam-video
model viv_media
serial
bus info
hw revision 0x0
driver version 5.15.52

Device topology
- entity 1: viv_v4l20 (1 pad, 1 link)
type Node subtype V4L flags 0
device node name /dev/video0
pad0: Sink
<- "vvcam-isp.0":0 [ENABLED]

- entity 5: vvcam-isp.0 (1 pad, 1 link)
type Node subtype V4L flags 0
device node name /dev/v4l-subdev0
pad0: Source
-> "viv_v4l20":0 [ENABLED]

- entity 7: vvcam-dwe.0 (2 pads, 0 link)
type Node subtype V4L flags 0
device node name /dev/v4l-subdev1
pad0: Source
pad1: Sink

 

My V4L2 output

root@edm-g-imx8mp:~# v4l2-ctl --list-devices
[ 2480.347798] enter isp_mi_stop
():
/dev/v4l-subdev0
/dev/v4l-subdev1

VIV (platform:viv0):
/dev/video0

viv_media (platform:vvcam-video):
/dev/media0

My Dts 

/dts-v1/;

#include "imx8mp-edm-g-wb.dts"

&i2c2 {
     /delete-node/ov5640_mipi@3c;
imx477_0: imx477@1a {
        compatible = "sony,imx477";
        reg = <0x1a>;
        pinctrl-names = "default";
        pinctrl-0 = <&pinctrl_csi0_pwn>, <&pinctrl_csi0_rst>, <&pinctrl_csi_mclk>;
        pwn-gpios = <&pca9555_a21 2 GPIO_ACTIVE_HIGH>;
        rst-gpios = <&gpio1 8 GPIO_ACTIVE_LOW>;
        clocks = <&clk IMX8MP_CLK_IPP_DO_CLKO2>;
        clock-names = "csi_mclk";
        assigned-clocks = <&clk IMX8MP_CLK_IPP_DO_CLKO2>;
        assigned-clock-parents = <&clk IMX8MP_CLK_24M>;
        assigned-clock-rates = <24000000>;
        mclk = <24000000>;
        mclk_source = <0>;
        mipi_csi;
        csi_id = <0>;

        status = "okay";

        port {
            imx477_0_ep: endpoint {
                data-lanes = <1 2>;
                clock-lanes = <0>;
                max-pixel-frequency = /bits/ 64 <500000000>;
                clock-noncontinuous;
                remote-endpoint = <&mipi_csi0_ep>;
            };
        };
    };
};

&i2c3 {
     clock-frequency = <100000>;
     pinctrl-names = "default";
     pinctrl-0 = <&pinctrl_i2c3>;
     status = "okay";
 
     ov5640_1: ov5640_mipi@3c {
         status = "disabled";
     };
 };
 
 &cameradev {
     status = "okay";
 };
 
 &isi_0 {
     status = "disabled";
 };
 
 &isi_1 {
     status = "disabled";
 };
 
 &isp_0 {
     status = "okay";
 };
 
 &dewarp {
     status = "okay";
 };

&mipi_csi_0 {
    status = "okay";
    #address-cells = <1>;
    #size-cells = <0>;
    clock-frequency = <500000000>;
    assigned-clock-rates = <500000000>;
    port@0 {
                reg = <0>;
                mipi_csi0_ep: endpoint {
                    remote-endpoint = <&imx477_0_ep>;
                    data-lanes = <1 2>;
                    csis-hs-settle = <13>;
                    csis-clk-settle = <1>;
                    csis-wclk;
                };
            };
};

&mipi_csi_1 {
     status = "disabled";
 };
 
ISI and VVCAM driver is attached 
 
Thank you,
Canberk
0 件の賞賛
返信
3 返答(返信)

3,536件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

3,531件の閲覧回数
CanberkOzbey
Contributor I
Hi Joanxie
Thanks for your reply but i already checked that link and it doesn't resolve my problem.
0 件の賞賛
返信

3,468件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

do you mind sharing the logfile with me? and pls refer to the enclosed application note, pls check if your setup is correct or not

0 件の賞賛
返信