Porting G2D to custom OS: where is G2D repository for i.MX7ULP ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Porting G2D to custom OS: where is G2D repository for i.MX7ULP ?

1,709 Views
ko-hey
Senior Contributor II

Hi all,

 

 

As we plan to port in-house kernel to i.MX7ULP to support 2D only applications, we would like to port G2D infrastructure.

Section 2.4 "Support of new operating system in G2D" of document "i.MX Graphics User's Guide" (ref. IMXGRAPHICUG Rev.2) tells about [G2D repository copy].

 

 

How can we retrieve this repository ?

Are there extra dependencies to be retrieved as well ?

 

 

Ko-hey

Labels (1)
Tags (3)
6 Replies

1,553 Views
radhikasomaiya
Senior Contributor II

Hi  ko-hey,

Yes, it is the same for i.MX7ULP you can refer to Table 3. BSP and Multimedia standard packages from attached i.MX Linux® Release Notes, Rev. L5.4.3_1.0.0, 03/2020.

You can also check ./meta-freescale/recipes-graphics/imx-gpu-g2d/imx-gpu-g2d_6.2.4.p4.0.bb file (GPU G2D library and apps for i.MX with 2D GPU and no DPU : i.MX Graphics G2D libraries are supported for both i.MX 6 and 7 with GPU).

g2d_6_7.png

Regards,

Radhika Somaiya.

0 Kudos
Reply

1,553 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Good!

1,553 Views
radhikasomaiya
Senior Contributor II

Hi ko-hey,

 

Can you please let us know that the link provided above is helpful to you or not?

Regards,

Radhika Somaiya.

0 Kudos
Reply

1,553 Views
ko-hey
Senior Contributor II

Hi Radhika Somaiya,

Is it same as for i.MX7ULP ?

if yes, it's helpful for us.

Ko-hey

0 Kudos
Reply

1,553 Views
radhikasomaiya
Senior Contributor II

Hi ko-hey,

Can you please provide us the detailed information like yocto version which you are using?

You can refer the below link

About G2D API in i.MX6DQ. 

I hope it can help you.

Regards,

Radhika Somaiya.

0 Kudos
Reply

1,553 Views
ko-hey
Senior Contributor II

Hi Radhika Somaiya

We're using L5.4.3_1.0.0.

Ko-hey

0 Kudos
Reply