Porting Android to a custom board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Porting Android to a custom board

跳至解决方案
1,414 次查看
pieter
Contributor II

Hi all!

I'm working on a custom iMX6 DL board. Can I use a pre-build Freescale Android BSP as a root filesystem for testing the GPU part of a kernel?

I'm curious if I can use this approach to validate proper operation of the GPU (e.g. finetune the kernel), or do I really need to create a custom Android BSP?

标签 (3)
0 项奖励
回复
1 解答
1,216 次查看
pieter
Contributor II

Ah, turns out you can! Just to be complete on this, I could test my custom kernel and custom device tree using both the Linux and the Android release root file system.


The Android root filesystem did need some tuning since I was using a NFS setup.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,217 次查看
pieter
Contributor II

Ah, turns out you can! Just to be complete on this, I could test my custom kernel and custom device tree using both the Linux and the Android release root file system.


The Android root filesystem did need some tuning since I was using a NFS setup.

0 项奖励
回复