Porting Android to a custom board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Porting Android to a custom board

ソリューションへジャンプ
1,941件の閲覧回数
pieter
Contributor II

Hi all!

I'm working on a custom iMX6 DL board. Can I use a pre-build Freescale Android BSP as a root filesystem for testing the GPU part of a kernel?

I'm curious if I can use this approach to validate proper operation of the GPU (e.g. finetune the kernel), or do I really need to create a custom Android BSP?

ラベル(3)
0 件の賞賛
返信
1 解決策
1,743件の閲覧回数
pieter
Contributor II

Ah, turns out you can! Just to be complete on this, I could test my custom kernel and custom device tree using both the Linux and the Android release root file system.


The Android root filesystem did need some tuning since I was using a NFS setup.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,744件の閲覧回数
pieter
Contributor II

Ah, turns out you can! Just to be complete on this, I could test my custom kernel and custom device tree using both the Linux and the Android release root file system.


The Android root filesystem did need some tuning since I was using a NFS setup.

0 件の賞賛
返信