Porting AGL(Automotive Grade Linux) onto I.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Porting AGL(Automotive Grade Linux) onto I.MX6

3,705 Views
saimadhusudhank
Contributor I

Hi ,

I want to port AGL on to our I.MX6 based board .Can any one suggest where to start and where to get the base Kernel package for it?

Reference for AGL

https://www.automotivelinux.org/

Thanks,

Saimadhusudhan

Labels (2)
2 Replies

1,632 Views
CarlChien
NXP Employee
NXP Employee

Hi Saimadhusudhan

Here are some informaito for your reference.

Regarding AGL, one demo is under NXP git sever. See http://git.freescale.com/git/cgit.cgi/imx/meta-nxp-agl.git/.

For details, you can refer to README http://git.freescale.com/git/cgit.cgi/imx/meta-nxp-agl.git/tree/README.txt?h=krogoth

 

Please note it’s demo, provided “as is”.

 

Best regards,

Carl

0 Kudos

1,632 Views
art
NXP Employee
NXP Employee

Various basic packages of i.MX6 Linux BSPs for various Linux kernel versions and i.MX6 processor types can be found here:

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos