Porting AGL(Automotive Grade Linux) onto I.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Porting AGL(Automotive Grade Linux) onto I.MX6

4,019 次查看
saimadhusudhank
Contributor I

Hi ,

I want to port AGL on to our I.MX6 based board .Can any one suggest where to start and where to get the base Kernel package for it?

Reference for AGL

https://www.automotivelinux.org/

Thanks,

Saimadhusudhan

标签 (2)
2 回复数

1,946 次查看
CarlChien
NXP Employee
NXP Employee

Hi Saimadhusudhan

Here are some informaito for your reference.

Regarding AGL, one demo is under NXP git sever. See http://git.freescale.com/git/cgit.cgi/imx/meta-nxp-agl.git/.

For details, you can refer to README http://git.freescale.com/git/cgit.cgi/imx/meta-nxp-agl.git/tree/README.txt?h=krogoth

 

Please note it’s demo, provided “as is”.

 

Best regards,

Carl

0 项奖励
回复

1,946 次查看
art
NXP Employee
NXP Employee

Various basic packages of i.MX6 Linux BSPs for various Linux kernel versions and i.MX6 processor types can be found here:

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复