Port of BCMDHD code modifications from i.MX7 to i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Port of BCMDHD code modifications from i.MX7 to i.MX6

1,815件の閲覧回数
CodeWarrior4_2M
Contributor II

Is there any reason to not port the following code modification on i.mx6?

linux-2.6-imx.git - Freescale i.MX Linux Tree

I am on the imx_3.14.38_6ul_ga and would expect the same type of update for the dts file like: imx6ul-14x14-evk.dts

Thanks for your comment

ラベル(4)
0 件の賞賛
返信
2 返答(返信)

1,567件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 79

one can try attached patch.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,567件の閲覧回数
mickaeltoumi
Contributor III

Thank Igor.

0 件の賞賛
返信