Hi,
I have enabled plymouth and dracut packages in my i.MX8M Yocto BSP (b2qt-embedded-qt5-image), with that I have also added a "quiet splash" in the kernel command line (/proc/cmdline). [ With reference to the following link : plymouth/dracut and i.mx6 ]
Note: Please find the screenshot in the attachment
Regards,
Ashok
Hello Ashok,
Plymouth recipe is available on the Yocto BSP as part of the OpenEmebedded layer.
http://layers.openembedded.org/layerindex/recipe/39966/
I would recommend you looking at the Plymouth homepage:
https://www.freedesktop.org/wiki/Software/Plymouth/
There are a couple of resources there that may be of help. As you dragcut there are some commands and more information on the dragcut documentation:
https://mirrors.edge.kernel.org/pub/linux/utils/boot/dracut/dracut.html#_dracut_8
Regards
Hi Bio_TICFSL,
I have gone through all the resource mentioned, and tried all the possibilites but results are same. I have no clue where I am missing.
Can you please provide clear procedure how plymouth to be added in yocto with configuration need to done initramfs and kernel command line.
Regards,
Ashok