-NXP iMX7
-Dual ARM Core A8+, 1Ghz+
-2 X 10/100 Eth Controllers MAC
-UARTS (5+)
-CAN( 1)
-SPI _ HS > 40Mhz (3), I2C(2)
-USB OTG/HS (1)
-OS: Linux
-Target cost b/w $10-$15 / 1K
-WiFi /BLE (Optional)
Hello,
Sorry, we do not have devices with Dual ARM Core A8.
Nevertheless, I think the mentioned i.MX7(D) is one of suitable candidates,
but its SPI is not so speedy as requested in Your parameters.
i.MX 7Dual Arm Cortex-A7 Processor|NXP
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------