Playing a specific Video using waylandsink not rendering under a wayland window

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Playing a specific Video using waylandsink not rendering under a wayland window

Jump to solution
5,703 Views
ArunkumarRajago
Contributor IV

Configure IMX8 with below.

  1. Configure Wayland with Desktop-shell and run the system(Wayland desktop will be shown).
  2. Play video.mp4(attached in this mail) with below pipeline

                gst-launch-1.0 filesrc location=video.mp4 ! decodebin3 ! imxvideoconvert_g2d ! queue ! waylandsink window-width=1280 window-height=480

 

  1. Now try to open weston-terminal, can be a button seen in left top corner in desktop window.

 

Issue is Weston-terminal cannot be moved on top of the video.

Understanding is video is rendered under a desktop wayland window. But it is not. we are not able to control the video window. Video rendering is blocking the behind desktop shell.

 

But if you open two Weston-terminal, you can control the view of windows by selecting through mouse.

We can understand that the video rendering directly to a plane on top of wayland o/p plane. But it should not be the case. How to solve this issue.

And we have integrated IVI_shell, want to control the video window.

Labels (1)
1 Solution
5,279 Views
danwei_luo
NXP Employee
NXP Employee

Hi Arunkumar Rajagopal,

The reason for the situation you saw is that Weston compositor will try to use DPU overlay to render videoplay by default. But it will put the videoplay on the top.

You can try following patch to disable using DPU overlay to render videoplay, then it will use GPU to render and fix the issue you saw.

diff --git a/libweston/compositor-drm.c b/libweston/compositor-drm.c
index 3365d29..b5bb9a4 100644
--- a/libweston/compositor-drm.c
+++ b/libweston/compositor-drm.c
@@ -3748,6 +3748,7 @@ drm_output_propose_state(struct weston_output *output_base,
struct weston_buffer *buffer = ev->surface->buffer_ref.buffer;
dmabuf = linux_dmabuf_buffer_get(buffer->resource);
if (dmabuf) {
+/*
if (dmabuf->attributes.format == DRM_FORMAT_NV12
|| dmabuf->attributes.format == DRM_FORMAT_P010
|| dmabuf->attributes.format == DRM_FORMAT_YUYV) {
@@ -3757,6 +3758,7 @@ drm_output_propose_state(struct weston_output *output_base,
else
force_renderer = true;
} else
+*/
force_renderer = true;
}
}

Apply the patch to weston-imx, recompile and replace drm-backend.so.

Best regards,

Danwei

View solution in original post

3 Replies
5,280 Views
danwei_luo
NXP Employee
NXP Employee

Hi Arunkumar Rajagopal,

The reason for the situation you saw is that Weston compositor will try to use DPU overlay to render videoplay by default. But it will put the videoplay on the top.

You can try following patch to disable using DPU overlay to render videoplay, then it will use GPU to render and fix the issue you saw.

diff --git a/libweston/compositor-drm.c b/libweston/compositor-drm.c
index 3365d29..b5bb9a4 100644
--- a/libweston/compositor-drm.c
+++ b/libweston/compositor-drm.c
@@ -3748,6 +3748,7 @@ drm_output_propose_state(struct weston_output *output_base,
struct weston_buffer *buffer = ev->surface->buffer_ref.buffer;
dmabuf = linux_dmabuf_buffer_get(buffer->resource);
if (dmabuf) {
+/*
if (dmabuf->attributes.format == DRM_FORMAT_NV12
|| dmabuf->attributes.format == DRM_FORMAT_P010
|| dmabuf->attributes.format == DRM_FORMAT_YUYV) {
@@ -3757,6 +3758,7 @@ drm_output_propose_state(struct weston_output *output_base,
else
force_renderer = true;
} else
+*/
force_renderer = true;
}
}

Apply the patch to weston-imx, recompile and replace drm-backend.so.

Best regards,

Danwei

5,279 Views
ArunkumarRajago
Contributor IV

Thanks Danwei,

We will try this patch and update here.

I have a question.

We understand, this drm based video rendering is basically for fast rendering. 

To keep this, Is there any configuration to render video in the bottom plane, when wayland o/p rendered at top plane.

So that we can configure wayland plane with colorkey configuration to make transparent and blend with video and render in the display.

Since wayland final display o/p pixel color cannot have alpha. so that we cannot use pixel alpha based blending.

Thanks,

Arunkumar R

0 Kudos
Reply
5,279 Views
danwei_luo
NXP Employee
NXP Employee

Hi Arunkumar Rajagopal,

Checked with R&D, currently using DPU to render video has to be done at top plane. So what you suggested cannot be done. But the performance of GPU rendering should be good as well.

Best regards,

Danwei