Hello everyone,
We are using an imx6solo custom board, which is using the SGTL5000 for internal speakers.
Using the command line, we are able to play two sounds at the same time on both the internal speakers and HDMI using tinyplay and stagefright.
We tried using ringtone and MediaPlayer, but the ringtone takes precedence over the MediaPlayer sound.
My question is then : is this feature available in Android, and if yes, in which version of the API.
Thank you guys
Solved! Go to Solution.
Hello Aebischer,
Try this patch, please! add it to your android manually!
Have a great day,
TIC weidong sun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Aebischer,
Try this patch, please! add it to your android manually!
Have a great day,
TIC weidong sun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you Weidong ! It's working perfectly fine :-)
Regards,
Quentin