Platform data with device tree

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Platform data with device tree

跳至解决方案
4,366 次查看
jeffrey_coffman
Contributor II

I'm in the process of upgrading from 3.0.35 to 4.1.15.  I am new to the world of device trees, etc..  I have a gpio expander chip pca9502 that I used to configure with platform data in a board configuration file, like so:

static const char* gpio_names[PCA9502_NUM_GPIO] = { "program",
NULL,
"soft_reset",
"flash_en",
"I0_L4N_T0_12",
"done",
"init_b",
"cpudone" };


static struct pca9502_platform_data pca9502_i2c_gpio_data = {
.num_gpio = PCA9502_NUM_GPIO,
.gpio_base = -1,
.names = gpio_names
};

Now I have moved to a device tree and have the following in my dts:

pca9502: pca9502@49 {
compatible = "nxp,pca9502";
reg = <0x49>;
gpio-controller;
};

What I am not sure about is now I pass platform data to the driver, now that I am using the device tree or if that is even possible.  Mainly I need .names for the gpios, and that used to get passed in platform data.  I've tried adding 

gpio-line-names property to my controller in the dts, but that doesn't seem to work or I misunderstand the kernel documentation in regard to it.

The gpios work fine other than they no longer have the aliased names in sysfs.

Is there a way to pass platform data without the old board descriptors in the newer kernel?  Otherwise is there a way to alias the names for controllers gpio lines like I used to be able to?

Thanks in advance.

标签 (1)
1 解答
3,018 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jeffrey

may be useful to check AN5125 Introduction to Device Trees

http://www.nxp.com/docs/en/application-note/AN5125.pdf 

parameters from dts can be passed in probe function

using of_property_read.. function as for example  in linux/drivers/gpio/gpio-pcf857x.c

linux-imx.git - i.MX Linux Kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
3,019 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jeffrey

may be useful to check AN5125 Introduction to Device Trees

http://www.nxp.com/docs/en/application-note/AN5125.pdf 

parameters from dts can be passed in probe function

using of_property_read.. function as for example  in linux/drivers/gpio/gpio-pcf857x.c

linux-imx.git - i.MX Linux Kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,018 次查看
jeffrey_coffman
Contributor II

Igor,

That worked perfectly for me!

Thank You,

Jeff

0 项奖励
回复