Hi NXP Team,
I am Planning to use MMPF0100F6ANES PMIC to support higher temperature range -40 to 105C with processor MCIMX6X1AVO08AC to support Ambient temperature range of -40 to 85C so is this preferable PMIC to use?
If yes, kindly share the associated design files.
If any other latest PMIC support available, please share the part detail and reference file.
PS: I have verified the latest SABRE BOARD EVK RevC PMIC details which is PF0200F6 but temperature range support is -40 to 85C.
Thank you,
Nilav Choksi
Hi Nilav Choksi,
You have two options:
If you choose this option, you can use the MCIMX6SX-SDB as a reference design since it is backward compatible with the PF0100 PMIC: https://www.nxp.com/design/development-boards/i.mx-evaluation-and-development-boards/sabre-board-for...
Regards,
Jose
NXP Semiconductors
Hi Jose Alberto,
Thank you for the reply.
I will use PF0100F6ANES PMIC and use MCIMX6SX-SDB (SPF-27962) REVC board design as a reference.
Thank you.