Hi all,
I am working on a custom board, which uses iMX6SoloX and Spansion S25FL512S QSPI flash device (active kernel is 3.14.28). There are a number of hurdles I have allready taken:
First off in uBoot, I have:
Then, in the kernel i have enable mtd and ubi in the config and made the following patched to the code
With these changes, my kernel boots with the following message:
[ 2.602850] UBI: attached mtd5 (name "Root Filesystem", size 56 MiB) to ubi0
[ 2.609914] UBI: PEB size: 262144 bytes (256 KiB), LEB size: 262016 bytes
[ 2.616752] UBI: min./max. I/O unit sizes: 1/512, sub-page size 1
[ 2.622869] UBI: VID header offset: 64 (aligned 64), data offset: 128
[ 2.629318] UBI: good PEBs: 224, bad PEBs: 0, corrupted PEBs: 0
[ 2.635254] UBI: user volume: 0, internal volumes: 1, max. volumes count: 128
[ 2.642410] UBI: max/mean erase counter: 0/0, WL threshold: 4096, image sequence number: 4284725391
[ 2.651474] UBI: available PEBs: 220, total reserved PEBs: 4, PEBs reserved for bad PEB handling: 0
[ 2.660532] UBI: background thread "ubi_bgt0d" started, PID 71
I can now succesfully ubiformat the /dev/mtd5 device, and then ubiattach it, and create a volume using ubimkvol
# ubimkvol /dev/ubi0 -m -N rootfs
Set volume size to 57643520
Volume ID 0, size 220 LEBs (57643520 bytes, 55.0 MiB), LEB size 262016 bytes (255.9 KiB), dynamic, name "rootfs", alignment
# ubinfo -a
UBI version: 1
Count of UBI devices: 1
UBI control device major/minor: 10:60
Present UBI devices: ubi0
ubi0
Volumes count: 0
Logical eraseblock size: 262016 bytes, 255.9 KiB
Total amount of logical eraseblocks: 224 (58691584 bytes, 56.0 MiB)
Amount of available logical eraseblocks: 220 (57643520 bytes, 55.0 MiB)
Maximum count of volumes 128
Count of bad physical eraseblocks: 0
Count of reserved physical eraseblocks: 0
Current maximum erase counter value: 1
Minimum input/output unit size: 1 byte
Character device major/minor: 248:0
Interesting to see is that LEB is 262016 bytes, which is 128 bytes shy of 256KiB (1/4 of my the s25fl512s page size!)
The (empty) volume I can succesfully mount using mount -t ubi0:rootfs /mnt, and I can then read/write to it just fine, and it will survive a reboot. Mounting gives me the following results:
# mount -t ubifs ubi0:rootfs /mnt/
[ 435.523097] UBIFS: default file-system created
[ 435.540930] UBIFS: background thread "ubifs_bgt0_0" started, PID 134
[ 435.607335] UBIFS: mounted UBI device 0, volume 0, name "rootfs"
[ 435.613676] UBIFS: LEB size: 262016 bytes (255 KiB), min./max. I/O unit sizes: 8 bytes/512 bytes
[ 435.622665] UBIFS: FS size: 55023360 bytes (52 MiB, 210 LEBs), journal size 2882176 bytes (2 MiB, 11 LEBs)
[ 435.632467] UBIFS: reserved for root: 2598889 bytes (2537 KiB)
[ 435.638314] UBIFS: media format: w4/r0 (latest is w4/r0), UUID 7B5FC98C-827F-4E68-A6A4-81FE5334C047, small LPT model
However, when I scp my rootfs.ubifs image across, and attempt to flash it with ubiupdatevol /dev/ubi0_0 rootfs.ubifs, I am less successful. The ubiupdatevol command passes nicely, but when I mount the partition same way as before, I get:
# ubiupdatevol /dev/ubi0_0 rootfs.ubifs
# mount -t ubifs ubi0:rootfs /mnt
[ 250.172597] UBIFS error (pid 148): validate_sb: min. I/O unit mismatch: 512 in superblock, 8 real
[ 250.190542] UBIFS error (pid 148): validate_sb: bad superblock, error 1
[ 250.202242] magic 0x6101831
[ 250.205914] crc 0x7f86c959
[ 250.209665] node_type 6 (superblock node)
[ 250.214243] group_type 0 (no node group)
[ 250.218605] sqnum 1
[ 250.221595] len 4096
[ 250.224827] key_hash 0 (R5)
[ 250.228231] key_fmt 0 (simple)
[ 250.232001] flags 0x0
[ 250.235145] big_lpt 0
[ 250.238112] space_fixup 0
[ 250.241096] min_io_size 512
[ 250.244240] leb_size 261632
[ 250.247642] leb_cnt 96
[ 250.250698] max_leb_cnt 96
[ 250.253768] max_bud_bytes 2877952
[ 250.257257] log_lebs 4
[ 250.260224] lpt_lebs 2
[ 250.263207] orph_lebs 1
[ 250.266176] jhead_cnt 1
[ 250.269145] fanout 8
[ 250.272127] lsave_cnt 256
[ 250.275270] default_compr 1
[ 250.278237] rp_size 0
[ 250.281219] rp_uid 0
[ 250.284188] rp_gid 0
[ 250.287155] fmt_version 4
[ 250.290122] time_gran 1000000000
[ 250.293889] UUID 438B6F15-EE7D-432B-9E9A-282B5B0ED9BD
mount: mounting ubi0:root on /mnt failed: Invalid argument
The following command was used to create rootfs.ubifs
mkfs.ubifs -d ./output/target -e 0x3fe00 -c 96 -m 0x200 -x lzo -o ./output/images/rootfs.ubifs
Here I specify 512 page size, and 255.5K LEB, which I believe to be correct for spansion s25fl512s device.
I seem to to be making a mistake in the generation of the ubifs, but who can help me specify the correct command line ?
I have also tried to set the page size to 128 byte, based on the output of ubinfo -a:
mkfs.ubifs -d ./output/target -e 0x3ff80 -c 96 -m 0x80 -x lzo -o ./output/images/rootfs.ubifs
But I get the same result - I/O unit real value is said to be only 8 - where is this defined ?
# mount -t ubifs ubi0:rootfs /mnt
[ 538.670907] UBIFS error (pid 161): validate_sb: min. I/O unit mismatch: 128 in superblock, 8 real
[ 538.679791] UBIFS error (pid 161): validate_sb: bad superblock, error 1
[ 538.697621] magic 0x6101831
[ 538.701341] crc 0xadede869
[ 538.705096] node_type 6 (superblock node)
[ 538.709628] group_type 0 (no node group)
[ 538.714008] sqnum 1
[ 538.716978] len 4096
[ 538.720207] key_hash 0 (R5)
[ 538.723627] key_fmt 0 (simple)
[ 538.727379] flags 0x0
[ 538.730520] big_lpt 0
[ 538.733504] space_fixup 0
[ 538.736473] min_io_size 128
[ 538.739614] leb_size 262016
[ 538.743032] leb_cnt 96
[ 538.746087] max_leb_cnt 96
[ 538.749141] max_bud_bytes 2882176
[ 538.752645] log_lebs 4
[ 538.755614] lpt_lebs 2
[ 538.758581] orph_lebs 1
[ 538.761564] jhead_cnt 1
[ 538.764532] fanout 8
[ 538.767500] lsave_cnt 256
[ 538.770641] default_compr 1
[ 538.773623] rp_size 0
[ 538.776592] rp_uid 0
[ 538.779559] rp_gid 0
[ 538.782543] fmt_version 4
[ 538.785512] time_gran 1000000000
[ 538.789265] UUID BB09566E-A88D-4D18-8FE3-CB4D9EEA8374
I found the cause of my headaches ...
As the S25FL512S is a NOR Flash, I need to create my ubifs with a Min IO size of 1 (not 512).
Also, I still need to take into account manually that the LEB is PEB - 128 bytes (2x 64byte for EC and VID header).
So, the command is :
mkfs.ubifs -d ./output/target -e 0x3ff80 -c 96 -m 0x1 -x lzo -o ./output/images/rootfs.ubifs
The generated rootfs.ubifs can be programmed using ubiupdatevol (but /dev/ubi must be ubiformatted first)
Alternatively, if I use ubinize to create rootfs.ubi, I can program this file directly when doing using ubiformat.
Note that I was not able to program the rootfs.ubi from uboot yet, as the .ubi file does not cover all erase-blocks (and each erase block needs at least the EC header). So I think I have some more work to do, to get ubi support for sf0 in uboot.
Hi Artur,
thanks for the parallel thread, but I could not find any usefull information in it, regarding UBIFS.
Re, Alexander