Pinmux Tool 2.0 generated files to u-boot config

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pinmux Tool 2.0 generated files to u-boot config

1,849件の閲覧回数
pyraohms
Contributor III

I need help with transferring the Pinmux 2.0 exported files and their data to files configuring u-boot (and possibly kernel) and generates the DTB-file. Any help would be appricieated. The EVK that we use is a imx6ul.

4 返答(返信)

1,593件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Per

one can follow uboot porting example on

U-Boot Migration Example 

setup code of reference board is already provided in u-boot../board/freescale/mx6ul_14x14_evk/mx6ul_14x14_evk.c

example of dts customization

http://boundarydevices.com/mx6-device-tree-customization/


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,593件の閲覧回数
pyraohms
Contributor III

Unfortunately, i can not make sense of the content. How does the general procedure for this go? Exporting PinMux 2.0 files and getting to a DTB file to put on SD-card?

0 件の賞賛
返信

1,593件の閲覧回数
pyraohms
Contributor III

Thanks. I'm new to this and in need of such

0 件の賞賛
返信