Pin mux discrepancy in IMX8DQXPRM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Pin mux discrepancy in IMX8DQXPRM

710 次查看
maximpodberezni
Contributor III

Hi!

found some discrepancy in IMX8DQXPRM pdf:

9.2.5.1.147 CSI_D00 (CSI_D00)

mux_mode
000b - CI_PI_CSI_D02
010b - ADMA_SAI0_RXC

9.2.5.1.148 CSI_D01 (CSI_D01)

mux_mode
000b - CI_PI_CSI_D03
010b - ADMA_SAI0_RXD

For CSI_D00 - pin mux description is for CI_PI_CSI_D02, for CSI_D01 - pin mux description is for CI_PI_CSI_D03, etc. Same issue is for all CSI_D00-CSI_D07. 

0 项奖励
回复
0 回复数