Pin mux Issue with gpio7[6]

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Pin mux Issue with gpio7[6]

1,140 次查看
akashgajjar
Contributor V

Hi all,

i have connected one sensor on  i2c 4 imx7d sabre board, gpio7[6] is used for reset

purpose, when i make gpio value 0 by

echo 0 > /sys/class/gpio198/value

my i2c4_scl comes to ground state.

here's device tree data

                pinctrl_i2c4: i2c4grp {                                         
                        fsl,pins = <                                            
                                MX7D_PAD_I2C4_SDA__I2C4_SDA     0x4000007f         
                                MX7D_PAD_I2C4_SCL__I2C4_SCL     0x4000007f         
                                MX7D_PAD_ENET1_RGMII_TD0__GPIO7_IO6        0x4000007f
                        >;                                                      
                };

when i detect the device it shows,

     0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f
00:          -- -- -- -- -- -- -- -- -- -- -- -- --
10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
70: -- -- -- -- -- -- -- --

when i2c 4 clock is at ground state it is scanning the device on bus as shown above,

can you please suggest me what's wrong with this.

Regards,

Akash

标签 (1)
4 回复数

892 次查看
akashgajjar
Contributor V

Hi Igor,

imx7d i2c controller is capable to drive the sccb supported sensor?

because both device has same sccb interface in camera.

Regards,

Akash

0 项奖励
回复

892 次查看
akashgajjar
Contributor V

HI igor,

This is sccb supported image sensor.

when i took out sensor device from the reset state this is happening.

can i access register of this device using i2c-tools from linux user-space?

Regards,

Akash

0 项奖励
回复

892 次查看
igorpadykov
NXP Employee
NXP Employee

could you try other sensor like ov5640, I believe line could be

hold by this specific sensor.

Best regards
igor

0 项奖励
回复

892 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Akash

seems low level is produced from sensor side, so one can check its pull resistors

and try to debug it with oscilloscope and probably temporarily cutting scl line.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------