Pin mapping of GPIO7 is missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pin mapping of GPIO7 is missing

ソリューションへジャンプ
1,755件の閲覧回数
K_Steinhammer
Contributor III

Where can I find the pin mapping of GPIO7 for the iMX8QM.

GPIO7 is defined in the address map, but there is no pin mapping defined in the Chip IO section of the SOCs reference manual.

As I am running out of GPIO pins, this information would be highly appreciated...

 

Thanks

0 件の賞賛
返信
1 解決策
1,739件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
2 返答(返信)
1,735件の閲覧回数
K_Steinhammer
Contributor III

OK, thanks for the confirmation...

0 件の賞賛
返信
1,740件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Yes, there is no GPIO7.

This is the pads of i.mx8qm defined in the bsp.

https://source.codeaurora.org/external/imx/linux-imx/tree/include/dt-bindings/pinctrl/pads-imx8qm.h?...

 

0 件の賞賛
返信