Pin functions of the OV5642 camera module for SABRE lite?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Pin functions of the OV5642 camera module for SABRE lite?

1,496 次查看
stephs
Contributor I

Are schematics available of the OV5642 camera module for SABRE lite?

I am interested in the mapping of the SABRE lite 33-pin J5 connector to the 24-pin connector of the imager module...

0 项奖励
回复
3 回复数

1,130 次查看
EricNelson
Senior Contributor II

Hello Stephs,

Schematics for the SABRE Lite are available in the support tab of our product page:

      http://boundarydevices.com/products/sabre-lite-imx6-sbc

1,130 次查看
stephs
Contributor I

Hi Eric,

thanks for the reply. I already found the schematics of the SABRE lite, and I also have the data sheet of the camera module.

Unfortunately, the information that I am looking for is missing.

I am looking for the connections on the little PCB that comes with the camera module, i.e. which signals of the 33-pin-connector are routed to which pins of the 24-pin-connector at the imager-side.

Kind regards,

Stephan

0 项奖励
回复

1,130 次查看
EricNelson
Senior Contributor II

Hi Stephs,

CSI0_D12-19, PIXCLK, VSYNC, HSYNC are connected to their respective pins on the Truly camera. GPIO3 is used to provide a clock, and the GPIOs are connected to enable and reset pins.

You can trace their functions in the camera driver in the Linux kernel, but it's likely that you'll need to re-map these to match your camera.

Regards,


Eric

0 项奖励
回复