Performance of rtsp server streaming with L4.1.15 on i.MX6 Dual

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Performance of rtsp server streaming with L4.1.15 on i.MX6 Dual

1,591件の閲覧回数
letan
Contributor III

Hello,

I have just upgrade up to L4.1.15 with imx-vpu-5.4.33 for our custom board(i.MX6 Dual).

Then the performance of the streaming is ~30fps without encryption. But actually when we run the streaming with libsrtp 1.5.3 and openssl encryption-enabled, the performance of the streaming downs to ~25-26fps.

Could you all please help me to clarify the problem?

Regards,

Tan

ラベル(3)
2 返答(返信)

1,431件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

In order to use OpenSSL engine, some changes should be provided in libsrtp.

Hope the following helps.

libsrtp / Mailing Lists

0 件の賞賛
返信

1,431件の閲覧回数
letan
Contributor III

That changes has already been there on openssl version 1.0.2. But how we know whether we are using hardware cryptodev while streaming or not?