Performance of rtsp server streaming with L4.1.15 on i.MX6 Dual

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Performance of rtsp server streaming with L4.1.15 on i.MX6 Dual

630 Views
letan
Contributor III

Hello,

I have just upgrade up to L4.1.15 with imx-vpu-5.4.33 for our custom board(i.MX6 Dual).

Then the performance of the streaming is ~30fps without encryption. But actually when we run the streaming with libsrtp 1.5.3 and openssl encryption-enabled, the performance of the streaming downs to ~25-26fps.

Could you all please help me to clarify the problem?

Regards,

Tan

Labels (3)
2 Replies

470 Views
jamesbone
NXP TechSupport
NXP TechSupport

In order to use OpenSSL engine, some changes should be provided in libsrtp.

Hope the following helps.

libsrtp / Mailing Lists

0 Kudos

470 Views
letan
Contributor III

That changes has already been there on openssl version 1.0.2. But how we know whether we are using hardware cryptodev while streaming or not?